SNVSBK9F November 2019 – September 2024 LM63635-Q1
PRODUCTION DATA
In some cases, an input UVLO level different than that provided internal to the device is needed. This need can be accomplished by using the circuit shown in Figure 8-3. The input voltage at which the device turns on is designated as VON while the turn-off voltage is VOFF. First, a value for RENB is chosen in the range of 10 kΩ to 100 kΩ. Then, Equation 12 is used to calculate RENT and VOFF.
where