SNVSCO0 January 2024 LM63635C-Q1
PRODUCTION DATA
In some cases, an input UVLO level different than that provided internal to the device is needed. This need can be accomplished by using the circuit shown in Figure 8-2. The input voltage at which the device turns on is designated as VON while the turnoff voltage is VOFF. First, a value for RENB is chosen in the range of 10kΩ to 100kΩ. Then, use Equation 9 to calculate RENT and VOFF.
where