SNVSCO0 January 2024 LM63635C-Q1
PRODUCTION DATA
In auto mode, the device moves between PWM and PFM as the load changes. At light loads, the regulator operates in PFM where the switching frequency is varied to regulate the output voltage. At higher loads, the mode changes to PWM with the switching frequency of the selected device.
In PWM mode, the regulator operates as a current mode, constant frequency converter using PWM to regulate the output voltage. While operating in this mode, the output voltage is regulated by switching at a constant frequency and modulating the duty cycle to control the power to the load. This action provides excellent line and load regulation and low output voltage ripple.
In PFM mode, the high-side MOSFET is turned on in a burst of one or more pulses to provide energy to the load. The duration of the burst depends on how long the inductor current takes to reach IPEAK-MIN. The periodicity of these bursts is adjusted to regulate the output, while diode emulation (DEM) is used to maximize efficiency (see the Glossary). This mode provides high light-load efficiency by reducing the amount of input supply current required to regulate the output voltage at small loads. This action trades off very good light-load efficiency for larger output voltage ripple and variable switching frequency. Also, a small increase in output voltage occurs at light loads. See Section 8.2.3 for output voltage variation with load in PFM mode. Figure 7-5 and Figure 7-6 show the typical switching waveforms in PFM and PWM.
There are four cases where the switching frequency does not conform to the condition set by the switching frequency:
Under all of these cases, the switching frequency folds back, meaning less than the programmed frequency. During these conditions, by definition, the output voltage remains in regulation, except for current limit operation.