SLVSEZ8A March 2019 – June 2019 LM66100
PRODUCTION DATA.
The shortcoming of the previous implementation happens when both input voltages are the same for a long period of time, then both devices will completely turn off, powering down the output load. To avoid this case, the status output from the priority supply and a pull up resistor can be used causing both devices to switchover at the same time. For ORing applications that need RPP, it is recommended to use a series resistor (RCE) to limit the current into the CE pin during a negative voltage event.