SNOSDB7 December 2020 LM74500-Q1
PRODUCTION DATA
PIN | I/O(1) | DESCRIPTION | |
---|---|---|---|
NO. | NAME | ||
1 | EN | I | Enable pin. Can be connected to SOURCE for always ON operation |
2 | GND | G | Ground pin |
3 | N.C | - | No connection |
4 | VCAP | O | Charge pump output. Connect to external charge pump capacitor |
5 | SOURCE | I | Input supply pin to the controller. Connect to the source of the external N-channel MOSFET |
6 | GATE | O | Gate drive output. Connect to gate of the external N-channel MOSFET |
7 | N.C | - | No connection |
8 | N.C | - | No connection |