Connect ANODE, GATE, and CATHODE pins of LM74703-Q1, LM74704-Q1 close to the SOURCE, GATE, and DRAIN pins of the MOSFET.
The high current path of this design is through the MOSFET, using thick traces for source and drain of the MOSFET to minimize resistive losses is important.
The charge pump capacitor across VCAP+ and VCAP– pins must be kept away from the MOSFET to lower the thermal effects on the capacitance value.
The GATE pin of the LM74703-Q1, LM74704-Q1 must be connected to the MOSFET gate with a short trace. Avoid excessively thin and long traces to the Gate Drive.
Keep the GATE pin close to the MOSFET to avoid increases in MOSFET turn-off delay due to trace resistance.
Obtaining acceptable performance with alternate layout schemes is possible, however the layout shown in the Layout Example is intended as a guideline and produces good results.