SNOSDE8A July 2023 – September 2023 LM74912-Q1
PRODUCTION DATA
LM74912-Q1 offers fast response to output short circuit events with the short circuit protection feature. The internal short circuit comparator is enabled when HGATE-OUT voltage is higher than 6.4-V typical. This is to ensure that external FET is fully enhanced and there are no false short circuit triggers during device start-up. When short circuit condition appears at the output and the voltage across CS+ and ISCP exceeds the default short circuit comparator threshold of 50-mV typical, HGATE is pulled to OUT within 2-µs protecting the HFET. FLT asserts low at the same time. Once short circuit condition is detected then device latches off MOSFET Q2 until either the EN, SLEEP or the VS pin is toggled from low to high.
Short circuit protection threshold can be increased or decreased from the default 50-mV threshold by using an external series resistor RSET from CS+ pin or RISCP from ISCP pin as shown in Figure 8-4. The RSET resistor shifts the threshold in positive direction while RISCP resistor shifts the threshold in negative direction. The shift in the short circuit protection threshold can be calculated using Equation 3 and Equation 4.
An additional de-glitch capacitor CISCP can be added from CS+ pin to ISCP pin as shown in Figure 8-4 to provide blanking on any short spurious current spikes to avoid false short circuit trigger in case of fast automotive transients such as Input Micro cuts (LV124, E-10), AC superimpose (LV124, E-06), ISO7637-2 Pulse 2A.
Also when MOSFET Q2 is turned off due to short circuit condition, there can be voltage oscillations on the supply line due to inductive effect of board parasitic and input wiring harness inductance. To avoid these oscillations from reaching to the device supply pin VS and causing false reset, additional series resistor RVS can be inserted. This series resistor RVS forms a R-C low pass filter with VS side decoupling capacitor CVS and helps with damping the oscillations.
The LM74912-Q1 is intended for applications where precise current sensing is not required, but some level of fault protection is needed. Examples are applications where inductance or impedance in the power path limits the current rise in a short circuit condition.
The Safe Operating Area (SOA) of the external N-Channel MOSFET must be carefully considered to make sure the peak drain-to-source current and the duration of the short circuit protection response time is within the SOA rating of the MOSFET. Also note that the RDS(ON) variations of the external N-Channel MOSFET over given temperature range affect the accuracy of the overcurrent detection.