SNOSDE8A July 2023 – September 2023 LM74912-Q1
PRODUCTION DATA
PIN | TYPE(1) | DESCRIPTION | |
---|---|---|---|
NAME | NO. | ||
DGATE | 1 | O | Diode controller gate drive output. Connect to the GATE of the external MOSFET. |
A | 2 | I | Anode of the ideal diode. Connect to the source of the external MOSFET. |
SW | 3 | I | Voltage sensing disconnect switch terminal. A and SW are internally connected through a switch. Use SW as the top connection of the battery sensing or OV resistor ladder network. When EN/SLEEP is pulled low, the switch is OFF disconnecting the resistor ladder from the battery line thereby cutting off the leakage current. If the internal disconnect switch between A and SW is not used then SW pin can be left floating or pulled to A. |
UVLO | 4 | I | Adjustable undervoltage threshold input. Connect a resistor ladder across SW to UVLO terminal to GND. When the voltage at UVLO goes below the undervoltage cut-off threshold then the HGATE is pulled low turning OFF the HSFET. HGATE turns ON when the sense voltage goes above the UVLO falling threshold. |
OV | 5 | I | Adjustable overvoltage threshold input. Connect a resistor ladder across SW to OV terminal. When the voltage at OV exceeds the overvoltage cut-off threshold then the HGATE is pulled low turning OFF the HSFET. HGATE turns ON when the sense voltage goes below the OV falling threshold. |
EN | 6 | I | EN input. Connect to VS pin for always ON operation. Can be driven externally from a micro controller I/O. Pulling it low below V(ENF) makes the device enter into low Iq shutdown mode. |
SLEEP | 7 | I | Active low SLEEP mode input. Can be driven from the micro-controller. When pulled low device enters into low power state with charge pump and gate drive turned off. Internal bypass switch provides output voltage with limited current capacity. When not used, should be tied to EN or VS. |
N.C. | 8 | — | No connection. Keep this pin floating. |
N.C. | 9 | — | No connection. Keep this pin floating. |
N.C. | 10 | — | No connection. Keep this pin floating. |
N.C. | 11 | — | No connection. Keep this pin floating. |
FLT | 12 | O | Open drain fault output. FLT pin is pulled low in case of undervoltage, overvoltage or output short circuit event. |
GND | 13 | G | Connect to the system ground plane. |
HGATE | 14 | O | GATE driver output for the HSFET. Connect to the GATE of the external FET. |
OUT | 15 | I | Connect to the output rail (external MOSFET source). |
SLEEP_OV | 16 | I | SLEEP mode over voltage protection pin. Connect this pin to Vs for over voltage cut-off functionality. Connect to OUT for over voltage clamp functionality. |
N.C. | 17 | — | No connection. Keep this pin floating. |
ISCP | 18 | I | Current sense negative input for adjustable short circuit protection. When ISCP is connected to output, device monitors external HFET voltage drop between CS+ and ISCP pins against an internal fix threshold of 50-mV typical. |
CS– | 19 | I | Current sense amplifier supply input. |
CS+ | 20 | I | Current sense positive input for adjustable short circuit protection. |
N.C. | 21 | — | No connection. Keep this pin floating. |
VS | 22 | P | Input power supply to the IC. Connect VS to middle point of the common drain back to back MOSFET configuration. Connect a 100-nF capacitor across VS and GND pins. |
CAP | 23 | O | Charge pump output. Connect a 100-nF capacitor across CAP and VS pin. |
C | 24 | I | Cathode of the ideal diode. Connect to the drain of the external MOSFET. |
RTN | Thermal pad | — | Leave exposed pad floating. Do not connect to GND plane. |