SNAS264D April 2006 – February 2024 LM94
PRODUCTION DATA
This function is very similar to the VRDx_HOT ramp-up/ramp-down function. The PWM duty cycle ramps up in the same fashion whenever the PROCHOT measurement exceeds the user programmed threshold. Once a new PROCHOT measurement is made that no longer exceeds the user limit, the PWM will begin to ramp down.
Just as with the VRDx_HOT ramp function, the PROCHOT ramp function uses independent bindings to determine which PWM outputs should be effected by each PROCHOT input ( P1_PROCHOT or P2_PROCHOT).
If a PWM is bound to both P1_PROCHOT and P2_PROCHOT, two PROCHOT ramp functions could be active at the same time. In this case the duty cycle that is used is the maximum of the two ramp functions.