SNAS264D April 2006 – February 2024 LM94
PRODUCTION DATA
The LM94 contains volatile registers, the registers occupy address locations from 00h to EFh.
Data can be read and written as a single byte, a word, or as a block of several bytes. The LM94 supports the following SMBus/I2C transactions/protocols:
In addition to these transactions the LM94 supports a few extra items and also has some behavior that must be defined beyond the SMBus 2.0 specification. No other SMBus 2.0 transactions are supported (PEC, ARA etc.).
The SMBus specification defines several protocols for different types of read and write operations. The ones used in the LM94 are discussed below. The following abbreviations are used in the diagrams: