SNAS264D April 2006 – February 2024 LM94
PRODUCTION DATA
Each time the LM94 is powered up, it latches the assigned SMBus slave address (determined by ADDR_SEL) during the first valid SMBus transaction in which the first five bits of the targeted slave address match those of the LM94 slave address. Once the address has been latched, the LM94 continues to use that address for all future transactions until power is lost.
The address select input detects three different voltage levels and allows for up to 3 devices to exist in a system. The address assignment is as follows:
Address Select Pin (ADDR_SEL) | Slave Address Assignment |
---|---|
High | 01011 01 |
VDD/2 | 01011 10 |
Low | 01011 00 |