SNAS264D April 2006 – February 2024 LM94
PRODUCTION DATA
Error Status registers function allow the LM94 to act as a legacy sensor (6.1.2 of ASF spec DSP0114 rev 2) and to easily connect to the SMBus of an ASF capable NIC chip.
The LM94 can be placed into ASF mode by setting the appropriate bit in the LM94 Status/Control register. Once this bit is set, the BMC Error Status registers become read-to-clear. Writing a ‘1’ to clear a particular bit is also allowed in ASF mode. The Host Error Status registers are not effected by ASF mode.