LM95231 always powers up to these known default states. The LM95231 remains in these states until after the first conversion.
- Command Register set to 00h
- Local Temperature set to 0°C until the end of the first conversion
- Remote Diode Temperature set to 0°C until the end of the first conversion
- Remote Diode digital filters are on.
- Remote Diode 1 model is set to Pentium 4 processor on 90nm process with TruTherm mode enabled. Remote Diode 2 model is set to 2N3904 with TruTherm mode disabled.
- Status Register depends on state of thermal diode inputs
- Configuration register set to 00h; continuous conversion, typical time = 85.8 ms when TruTherm Mode is enabled for Remote 1 only