The actual component values
represented in bold of Figure 7-7 were obtained with the following scaling procedure:
- First determine the frequency
scaling factor (FSF) for the desired cutoff frequency. Choosing fc at
3kHz, provides the following FSF computation:
Equation 1.
- Then divide all of the normalized
capacitor values by the FSF as follows (C1' and C2': prior to impedance
scaling):
Equation 2.
Equation 3.
- Last, choose an impedance scaling
factor (Z). This Z factor can be calculated from a standard value for C2. Then Z
can be used to determine the remaining component values as follows:
Equation 4.
Equation 5.
Equation 6.
Equation 7.
- A standard value of 8.45kΩ is chosen for R1 and R2.