SNOSA83I August 2003 – August 2014 LMH6723 , LMH6724
PRODUCTION DATA.
Follow these steps to determine the maximum power dissipation for the LMH6723/LMH6724:
where VS = V+ - V-
The maximum power that the LMH6723/LMH6724 package can dissipate at a given temperature can be derived with the following equation:
where
For the SOIC-8 package RθJA is 166°C/W and for the SOT-23-5 it is 230°C/W.
The LMH6723/LMH6724 is protected against electrostatic discharge (ESD) on all pins. The LMH6723 will survive 2000V Human Body Model or 200V Machine Model events.
Under closed loop operation the ESD diodes have no effect on circuit performance. There are occasions, however, when the ESD diodes will be evident. If the LMH6723/LMH6724 is driven into a slewing condition the ESD diodes will clamp large differential voltages until the feedback loop restores closed loop operation. Also, if the device is powered down and a large input signal is applied, the ESD diodes will conduct.