SNAS841 October 2023 LMK04714-Q1
PRODUCTION DATA
In general, the following general guidelines are useful to keep in mind.
In addition to this, there are special considerations for the routing of the outputs. The outputs are divided in to several output groups.
It is optimal to isolate the power supply pins for these clock group pins with a ferrite bead to crosstalk between the outputs, especially if the output groups have different frequencies. If there is flexibility in planning which frequencies go to which outputs, crosstalk can be minimized by putting different frequencies in different output groups (as opposed to putting them in the same output group).