When TOD_CNTR_TRIG is 1 (GPIO pin):
- Timing accuracy of 1 ToD cycle + 2 ns requires a 20% to 80% rise time of
less than or equal to 1 ns.
- GPIOx rising edge should not
occur within 10 ns of rising SCS which sets TOD_CNTR_EN from 0 to 1.
- GPIOx should remain high for 10 ns.
- A new GPIOx trigger should
not arrive within 1 µs of the rising edge of the SPI SCS
after reading the LSB of the TOD_CNTR.
When TOD_CNTR_TRIG is 0 (SPI):
- Timing accuracy of 1 ToD cycle + 2 ns requires an 80% to 20% fall time of
less than or equal to 1 ns.
- The ToD counter is captured
to the TOD_CNTR registers at the falling edge of SPI SCS. No additional time
to read back or pre-latching of register is required.