SNAS633A March 2014 – September 2014 LMP93601
PRODUCTION DATA.
To achieve high noise performance of the LMP93601, particular attention must be paid to the layout of the input signals, inputs INPx and INNx. To avoid introduction of differential noise into the pins, the input traces must lay out symmetrically.
Proper power-supply decoupling is required on both AVDD and IOVDD. The Supply pins should be decoupled with at least a 0.1 μF bypass capacitor each. The bypass capacitors should be placed as close to the power-supply pins as possible with a low impedance connection. For very sensitive systems, or for systems in harsh noise environments, avoiding the use of vias for connecting the bypass capacitor may offer superior bypass and noise immunity.
It is recommended that in the layout, analog components [such as ADCs, amplifiers, references, digital-to-analog converters (DACs), and analog MUXs] be separated from digital components [such as microcontrollers, complex programmable logic devices (CPLDs), field-programmable gate arrays (FPGAs), radio frequency (RF) transceivers, universal serial bus (USB) transceivers, and switching regulators]. The best placement for each application is unique to the geometries, components, and PCB fabrication capabilities employed. That is, there is no single layout that is perfect for every design and careful consideration must always be used when designing with any analog component.
TI recommends placing 47 Ω resistors in series with all digital input and output pins (CS, SCLK, DIN, DOUT/DRDY, and DRDY). This resistance smooths sharp transitions, suppresses overshoot, and offers some overvoltage protection. Care must be taken to still meet all SPI timing requirements because the additional resistors interact with the bus capacitances present on the digital signal lines.
TI also strongly recommends that digital components, especially RF portions, be kept as far as practically possible from analog circuitry in a given system. Additionally, one should minimize the distance that digital control traces run through analog areas and avoid placing these traces near sensitive analog components. Digital return currents usually flow through a ground path that is as close as possible to the digital path. If a solid ground connection to a plane is not available, these currents may find paths back to the source that interfere with analog performance. The implications that layout has on the temperature-sensing functions are much more significant than for ADC functions.
The internal ADC reference supply of the LMP93601 requires a 1 µF high performance (low ESR & ESL) cap on the XCAP1. This cap must be placed in the immediate proximity of the pin. For best performance it is recommended that the DAP be connected to AGND. All three "GND" connections (AGND, DGND, and IOGND) must be connected to system ground and cannot be left floating.