The PCB layout of any DC/DC converter is critical
to the optimal performance of the design. Bad PCB layout can disrupt the operation of an
otherwise good schematic design. Even if the converter regulates correctly, bad PCB layout
can mean the difference between a robust design and one that cannot be mass produced.
Furthermore, the EMI performance of the regulator is dependent on the PCB layout, to a great
extent. In a buck converter, the most critical PCB feature is the loop formed by the input
capacitor or input capacitors, and power ground, as shown in Figure 8-15. This loop carries large
transient currents that can cause large transient voltages when reacting with the trace
inductance. These unwanted transient voltages disrupt the proper operation of the converter.
Because of this, the traces in this loop must be wide and short, and the loop area as small
as possible to reduce the parasitic inductance. Section 8.5.2 shows a recommended layout for the critical components of the LMR38015.
- Place the input capacitors as close as
possible to the VIN pins and connect to ground through a short wide trace.
- Apply the symmetrical input capacitors
technique as shown in the LMR38025EVQM
- Use wide traces for the CBOOT
capacitor. Place CBOOT close to the device with short/wide traces to the
BOOT and SW pins. The BOOT and SW pins are adjacent which simplifies the CBOOT
capacitor placement.
- Place the feedback divider as close as
possible to the FB pin of the device. Place RFBB, RFBT, and
CFF, if used, physically close to the device. The connections to FB and GND
must be short and close to those pins on the device. The connection to VOUT can
be somewhat longer. However, this latter trace must not be routed near any noise sources
(such as the SW node) that can capacitively couple into the feedback path of the
regulator.
- Use at least one ground plane in one of the middle layers. This plane acts as a noise shield and also act as a heat dissipation path.
- Connect the thermal pad to the ground
plane. The WSON package has a thermal pad (PAD) connection that can be soldered down
to the PCB ground plane. This pad acts as a heat-sink connection. The integrity of this
solder connection has a direct bearing on the total effective RθJA of the
application.
- Provide wide planes for VIN, VOUT, and
GND. Making these paths as wide and direct as possible reduces any voltage drops on
the input or output paths of the converter and maximizes efficiency.
- Provide enough PCB area for proper heat
sinking. Enough copper area must be used to keep a low RθJA, commensurate
with the maximum load current and ambient temperature. Make the top and bottom PCB layers
with two-ounce copper; and no less than one ounce. With the WSON package, use at least
three heat-sinking vias to connect the thermal pad (PAD) to the ground plane on the
bottom PCB layer. If the PCB design uses multiple copper layers (recommended),
thermal vias can also be connected to the inner layer heat-spreading ground planes.
- Keep switch area small. Keep the copper
area connecting the SW pin to the inductor as short and wide as possible. At the same time
the total area of this node must be minimized to help reduce radiated EMI.
See the following PCB layout resources for additional important guidelines: