SNVSCM5 January 2024 LMR43606-Q1
PRODUCTION DATA
As with any power conversion device, the LMR43606-Q1 dissipates internal power while operating. The effect of this power dissipation is to raise the internal temperature of the converter above ambient. The internal die temperature (TJ) is a function of the ambient temperature, the power loss, and the effective thermal resistance, RθJA, of the device, and PCB combination. The maximum junction temperature for the LMR43606-Q1 must be limited to 150°C. This limit establishes a limit on the maximum device power dissipation and, therefore, the load current. Equation 13 shows the relationships between the important parameters. Seeing that larger ambient temperatures (TA) and larger values of RθJA reduce the maximum available output current is easy. The converter efficiency can be estimated by using the curves provided in this data sheet. If the desired operating conditions cannot be found in one of the curves, interpolation can be used to estimate the efficiency. Alternatively, the EVM can be adjusted to match the desired application requirements and the efficiency can be measured directly. The correct value of RθJA is more difficult to estimate. For more information reference Semiconductor and IC Package Thermal Metrics application report.
where
The effective RθJA is a critical parameter and depends on many factors such as the following:
Use Equation 14 to estimate the IC junction temperature for a given operating condition.
where
The IC Power loss mentioned above is the overall power loss minus the loss that comes from the inductor DC resistance. The overall power loss can be approximated by using WEBENCH for a specific operating condition and temperature.
Use the following resources as guides to optimal thermal PCB design and estimating RθJA for a given application environment: