SNVSCM5 January 2024 LMR43606-Q1
PRODUCTION DATA
In some cases, an input UVLO level different than that provided internal to the device is needed. This level can be accomplished by using the circuit shown in Figure 8-2. The input voltage at which the device turns on is designated as VON while the turn-off voltage is VOFF. First, a value for RENB is chosen in the range of 10kΩ to 100kΩ, then Equation 11 and Equation 12 are used to calculate RENT and VOFF respectively.
where