Layout is a critical portion of good power supply
design. The following guidelines help users design a PCB with the best power
conversion performance, thermal performance, and minimized generation of unwanted
EMI.
- The input bypass capacitor CIN must be
placed as close as possible to the VIN and PGND pins. Grounding for both the
input and output capacitors must consist of localized top side planes that
connect to the PGND pin.
- Minimize trace length to the FB pin net. Both feedback resistors, RFBT and RFBB, must be located close to the FB pin. If VOUT accuracy at the load is important, make sure VOUT sense is made at the load. Route VOUT sense path away from noisy nodes and preferably through a layer on the other side of a shielded layer.
- Use ground plane in one of the middle layers as noise shielding and heat dissipation path if possible.
- Make VIN, VOUT, and ground bus connections as wide as possible. This reduces any voltage drops on the input or output paths of the converter and maximizes efficiency.
- Provide adequate device heat-sinking. Use an
array of heat-sinking vias to connect the top side ground plane to the ground
plane on the bottom PCB layer. If the PCB has multiple copper layers, these
thermal vias can also be connected to inner layer heat-spreading ground planes.
Make sure enough copper area is used for heat-sinking to keep the junction
temperature below 150°C.