SNAS872 December 2024 LMR60410
PRODMIX
The LMR60410 implements a feedback impedance detect circuitry which allows for users to configure the output voltage of the LMR60410 to be either fixed or adjustable depending on the presence of a feedback resistor divider connected to the FB pin. The fixed output voltage is determined based on the orderable part number, see Section 4 for details. If fixed output voltage is desired, the FB pin can be shorted directly to the output voltage rail. There must be less than 25Ω between the FB pin and the output voltage rail for the device to enter into fixed output voltage. If an adjustable output voltage is desired, the parallel combination of the top and bottom feedback resistors must exceed 1100Ω. After the top feedback resistor is selected, RFBT, Equation 4 can be used to select the bottom feedback resistor, RFBB.
Where VFB is typically 1V and RFBT is typically selected to be 100kΩ.