SNAS872 December 2024 LMR60410
PRODMIX
A resistor placed between the RT pin and PGND is used to select the set point switching frequency of the LMR60410 typically between 200kHz and 2.2MHz. The set point switching frequency represents the switching frequency which occurs if the LMR60410 were operating in continuous conduction mode with spread spectrum disabled. Refer to Section 7.3.9 for more information on how spread spectrum affects the switching frequency. Equation 3 can be used to determine the RT resistor value for a desired set point switching frequency.
Where: