SNAS851 December 2023 LMX1906-SP
PRODUCTION DATA
The state machine clock frequency (fSMCLK) is derived by dividing down the input clock frequency by a programmed divider value. The state machine clock is also necessary for the multiplier calibration and lock detect. If there are concerns about the state machine clock creating spurs, then the state machine clock can be shut off, provided that the multiplier calibration is not running and the lock detect feature is not in use.