SNAS739D June 2018 – May 2020 LMX2615-SP
PRODUCTION DATA.
MODE | DESCRIPTION | SOFTWARE SETTINGS |
---|---|---|
RESET | Registers are held in their reset state. This device does have a power on reset, but it is good practice to also do a software reset if there is any possibility of noise on the programming lines, especially if there is sharing with other devices. Also realize that there are registers not disclosed in the data sheet that are reset as well. | RESET = 1
POWERDOWN = 0 |
POWERDOWN | Device is powered down. | POWERDOWN = 1
or CAL Pin = Low |
Pin Mode | Device settings are determined by pin states. | One of FS0, FS1, ... FS7 pins is NOT low |
Normal operating mode | This is used with at least one output on as a frequency synthesizer and the device can be controlled through the SPI interface | ALL of FS0, FS1, ... FS7 pins are low |
SYNC mode | This is used where part of the channel divider is in the feedback path to ensure deterministic phase. | VCO_PHASE_SYNC = 1 |
SYSREF mode | In this mode, RFoutB is used to generate pulses for SYSREF. | VCO_PHASE_SYNC =1, SYSREF_EN = 1 |