7.3.16 Pin Modes
The LMX2615-SP has 8 pins that can be used to program pre-selected modes. A few rules of operation for these pin modes are as follows:
- Set the pin mode as desired. Pin Mode 0 is SPI mode
- If a single frequency is desired, tie CAL should be tied to supply through 1-kΩ resistance and RECAL_EN should be left open.
- The rise time for the supply needs to be <50 ms.
- Fractional denominator for all pin modes is 4250000
- Some words can be overwritten in pin mode including OUTx_PWR, OUTx_EN, RESET, and POWERDOWN
When changing between pin modes, after the pins are changed, the CAL pin must be toggled.
- If the FS7 pin is low, then only the RFoutA output is active. If the FS7 pin is high, then both the RFoutA and RFoutB outputs are active.
The following table shows all the pin modes
Table 17. Pin Modes
MODE |
fOSC
(MHz) |
fPD
(MHz) |
CPG
(mA) |
fOUT
(MHz) |
CHDIV |
fVCO
(MHz) |
N |
FRACTION |
0 |
SPI Mode |
1 |
10 |
20 |
15 |
160 |
48 |
7680 |
384 |
0/4250000000 |
2 |
10 |
10 |
15 |
395 |
24 |
9480 |
948 |
0/4250000000 |
3 |
10 |
20 |
15 |
720 |
12 |
8640 |
432 |
0/4250000000 |
4 |
10 |
20 |
15 |
1280 |
6 |
7680 |
384 |
0/4250000000 |
5 |
100 |
200 |
15 |
300 |
32 |
9600 |
48 |
0/4250000000 |
6 |
100 |
200 |
15 |
1000 |
8 |
8000 |
40 |
0/4250000000 |
7 |
100 |
200 |
15 |
1200 |
8 |
9600 |
48 |
0/4250000000 |
8 |
20 |
40 |
15 |
6199.855 |
2 |
12399.71 |
309 |
4219187500/4250000000 |
9 |
100 |
200 |
15 |
2000 |
4 |
8000 |
40 |
0/4250000000 |
10 |
50 |
100 |
15 |
250 |
32 |
8000 |
80 |
0/4250000000 |
11 |
50 |
100 |
15 |
500 |
16 |
8000 |
80 |
0/4250000000 |
12 |
50 |
100 |
15 |
850 |
12 |
10200 |
102 |
0/4250000000 |
13 |
20 |
40 |
15 |
5654.912 |
2 |
11309.824 |
282 |
3168800000/4250000000 |
14 |
10 |
20 |
15 |
1517.867839 |
6 |
9107.207034 |
455 |
1531494725/4250000000 |
15 |
10 |
20 |
15 |
1708.670653 |
6 |
10252.02392 |
512 |
2555082575/4250000000 |
16 |
50 |
100 |
15 |
2500 |
4 |
10000 |
100 |
0/4250000000 |
17 |
Reserved. Do not use this pin mode. |
18 |
10 |
20 |
15 |
3035.735678 |
4 |
12142.94271 |
607 |
625326300/4250000000 |
19 |
50 |
100 |
15 |
3200 |
4 |
12800 |
128 |
0/4250000000 |
20 |
10 |
20 |
15 |
3417.341306 |
4 |
13669.36522 |
683 |
1990110100/4250000000 |
21 |
50 |
100 |
15 |
4500 |
2 |
9000 |
90 |
0/4250000000 |
22 |
50 |
100 |
15 |
4800 |
2 |
9600 |
96 |
0/4250000000 |
23 |
50 |
100 |
15 |
5350 |
2 |
10700 |
107 |
0/4250000000 |
24 |
50 |
100 |
15 |
6800 |
2 |
13600 |
136 |
0/4250000000 |
25 |
10 |
20 |
15 |
6834 |
2 |
13668 |
683 |
1700000000/4250000000 |
26 |
10 |
20 |
15 |
6834.682611 |
2 |
13669.36522 |
683 |
1990109675/4250000000 |
27 |
10 |
20 |
15 |
6834.6875 |
2 |
13669.375 |
683 |
1992187500/4250000000 |
28 |
10 |
20 |
15 |
6834.75 |
2 |
13669.5 |
683 |
2018750000/4250000000 |
29 |
50 |
100 |
15 |
9600 |
1 |
9600 |
96 |
0/4250000000 |
30 |
50 |
100 |
15 |
9650 |
1 |
9650 |
96 |
2125000000/4250000000 |
31 |
50 |
100 |
15 |
13500 |
1 |
13500 |
135 |
0/4250000000 |
32 |
100 |
100 |
15 |
70 |
128 |
8960 |
89 |
2550000000/4250000000 |
33 |
18.75 |
37.5 |
15 |
393.75 |
24 |
9450 |
252 |
0/4250000000 |
34 |
18.75 |
37.5 |
15 |
422.4990441 |
24 |
10139.97706 |
270 |
1697399952/4250000000 |
35 |
37.5 |
75 |
15 |
422.4990441 |
24 |
10139.97706 |
135 |
848699976/4250000000 |
36 |
20 |
40 |
15 |
6785.552 |
2 |
13571.104 |
339 |
1179800000/4250000000 |
37 |
20 |
40 |
15 |
2088.38 |
4 |
8353.52 |
208 |
3561500000/4250000000 |
38 |
100 |
100 |
15 |
2210 |
4 |
8840 |
88 |
1700000000/4250000000 |
39 |
100 |
100 |
15 |
2238 |
4 |
8952 |
89 |
2210000000/4250000000 |
40 |
20 |
40 |
15 |
2254.35 |
4 |
9017.4 |
225 |
1848750000/4250000000 |
41 |
20 |
40 |
15 |
2270 |
4 |
9080 |
227 |
0/4250000000 |
42 |
20 |
40 |
15 |
2280 |
4 |
9120 |
228 |
0/4250000000 |
43 |
18.75 |
37.5 |
15 |
6759.984705 |
2 |
13519.96941 |
360 |
2263199800/4250000000 |
44 |
37.5 |
75 |
15 |
6759.984705 |
2 |
13519.96941 |
180 |
1131599900/4250000000 |
45 |
20 |
40 |
15 |
8125 |
1 |
8125 |
203 |
531250000/4250000000 |
46 |
20 |
40 |
15 |
8175 |
1 |
8175 |
204 |
1593750000/4250000000 |
47 |
20 |
40 |
15 |
8200 |
1 |
8200 |
205 |
0/4250000000 |
48 |
20 |
40 |
15 |
8210 |
1 |
8210 |
205 |
1062500000/4250000000 |
49 |
20 |
40 |
15 |
8212.5 |
1 |
8212.5 |
205 |
1328125000/4250000000 |
50 |
20 |
40 |
15 |
8275 |
1 |
8275 |
206 |
3718750000/4250000000 |
51 |
20 |
40 |
15 |
8300 |
1 |
8300 |
207 |
2125000000/4250000000 |
52 |
20 |
40 |
15 |
8400 |
1 |
8400 |
210 |
0/4250000000 |
53 |
20 |
40 |
15 |
8450 |
1 |
8450 |
211 |
1062500000/4250000000 |
54 |
20 |
40 |
15 |
8460 |
1 |
8460 |
211 |
2125000000/4250000000 |
55 |
20 |
40 |
15 |
8484 |
1 |
8484 |
212 |
425000000/4250000000 |
56 |
20 |
40 |
15 |
8496 |
1 |
8496 |
212 |
1700000000/4250000000 |
57 |
20 |
40 |
15 |
8212 |
1 |
8212 |
205 |
1275000000/4250000000 |
58 |
10 |
20 |
15 |
12860 |
1 |
12860 |
643 |
0/4250000000 |
59 |
10 |
20 |
15 |
13000 |
1 |
13000 |
650 |
0/4250000000 |
60 |
10 |
20 |
15 |
13022.5 |
1 |
13022.5 |
651 |
531250000/4250000000 |
61 |
10 |
20 |
15 |
13125 |
1 |
13125 |
656 |
1062500000/4250000000 |
62 |
10 |
20 |
15 |
13222.5 |
1 |
13222.5 |
661 |
531250000/4250000000 |
63 |
20 |
40 |
15 |
12209.697 |
1 |
12209.697 |
305 |
1030306250/4250000000 |
64 |
10 |
20 |
15 |
13390 |
1 |
13390 |
669 |
2125000000/4250000000 |
65 |
10 |
20 |
15 |
13417.5 |
1 |
13417.5 |
670 |
3718750000/4250000000 |
66 |
20 |
40 |
15 |
12689.697 |
1 |
12689.697 |
317 |
1030412500/4250000000 |
67 |
20 |
40 |
15 |
13906.667 |
1 |
13906.667 |
347 |
2833368750/4250000000 |
68 |
20 |
40 |
15 |
14192.727 |
1 |
14192.727 |
354 |
3477243750/4250000000 |
69 |
10 |
20 |
15 |
8212.5 |
1 |
8212.5 |
410 |
2656250000/4250000000 |
70 |
100 |
50 |
15 |
1250 |
8 |
10000 |
200 |
0/4250000000 |
71 |
50 |
100 |
15 |
1250 |
8 |
10000 |
100 |
0/4250000000 |
72 |
18.75 |
37.5 |
15 |
1875 |
6 |
11250 |
300 |
0/4250000000 |