For the most reliable programming, TI recommends this procedure:
- Apply power to device.
- Program RESET = 1 to reset registers.
- Program RESET = 0 to remove reset.
- Program registers as shown in the register map in REVERSE order from highest to lowest.
- Programming of registers R113 down to R79 is not required, but if they are programmed, they should be done so as the register map shows. Programming of registers R79 down to R0 is required. Registers in this range that only 1's and 0's should also be programmed in accordance to the register map. Do NOT assume that the power-on reset state and the recommended value are the same.
- Wait 10 ms.
- Program register R0 one additional time with FCAL_EN = 1 to ensure that the VCO calibration runs from a stable state.