SNAS783C June 2020 – February 2021 LMX2820
PRODUCTION DATA
Instant calibration allows the device to very quickly calibrate the VCO in 2.5 µs and choose the same calibration settings (rb_VCO_SEL, rb_VCO_DACISET, rb_VCO_CAPCTRL). Once this feature is initialized, then there is no overhead in changing the VCO frequency. This initialization is required when the device is initially powered up, but the settings are retained, provided power is not removed from the supply pins. The following procedure details how this is done:
| PIN 3 CAPACITANCE | PLL 1/f NOISE DEGRADATION | MINIMUM tDLY |
|---|---|---|
| 0.47 μF | 1 dB | 2.5 μs |
| C | 0-1 dB | 2.5 μs × C/(0.47 μF) |
| 4.7 μF | 0 dB | 25 μs |
Now the device is initialized for the particular phase detector frequency that this was done at. Provided that power is not removed from the device and then phase detector frequency does not change, subsequent frequency changes an be done using the instant cal. To change frequencies after the instant calibration is initialized: