SNVS542E May 2008 – June 2016 LP8900
PRODUCTION DATA.
The dynamic performance of the LP8900 is dependant on the layout of the PCB. PCB layout practices that are adequate for typical LDOs may degrade the PSRR, noise, or transient performance of the LP8900.
Best performance is achieved by placing CIN and COUT on the same side of the PCB as the device, and placing them as close as is practical to the package. The ground connections for CIN and COUT must be back to the LP8900 ground pin using as wide and as short of a copper trace as is practical.
Connections using long trace lengths, narrow trace widths, and/or connections through vias must be avoided. These add parasitic inductances and resistance that results in inferior performance especially during transient conditions.
The DSBGA package requires specific mounting techniques which are detailed in the TI Application Note (AN-1112) DSBGA Wafer Level Chip Scale Package (SNVA009). Referring to the section Surface Mount Technology (SMT) Assenbly Considerations, the pad style that must be used with the 6-pin package is a NSMD (non-solder mask defined) type.
For best results during assembly, alignment ordinals on the PCB may be used to facilitate placement of the DSBGA device.
Exposing the DSBGA device to direct sunlight may cause mis-operation of the device. Light sources such as halogen lamps can affect the electrical performance if brought near to the device.
The wavelengths that have the most detrimental effect are reds and infra-reds, which means that the fluorescent lighting used inside most buildings has little effect on performance.