SLLSFQ7 November 2023 MCF8329A
PRODUCTION DATA
The MCF8329A uses the motor resistance, motor inductance and motor back-EMF constant to estimate motor position when operating in closed loop. The MCF8329A has the capability of measuring motor back-EMF constant in the offline state (see Motor Parameter Extraction Tool (MPET)). Offline measurement of motor back-EMF constant, when enabled, takes place before normal motor operation. The user can also disable the offline measurement and configure motor parameters through EEPROM. This feature of offline motor parameter measurement is useful to account for motor to motor variation during manufacturing.