Staircase control profiles can be configured by
setting REF_PROFILE_CONFIG to 10b. Staircase profiles feature input control
reference changes in steps between REF_CLAMP1 and REF_CLAMP2, by configuring DUTY_x
and REF_x.
- DUTY_OFF1 configures the duty command below which the reference will be
REF_OFF1.
- DUTY_OFF1 and DUTY_ON1configures a hysteresis around
reference control input REF_CLAMP1 and REF_OFF1 as shown in Figure 7-12.
- DUTY_CLAMP1 configures the duty command till
which reference will be constant. REF_CLAMP1 configures this constant
reference between DUTY_OFF1 and DUTY_CLAMP1. DUTY_CLAMP1 can be placed
anywhere between DUTY_OFF1 and DUTY_A.
- DUTY_A configures the duty command for reference
REF_A. There is a step change in reference from REF_CLAMP1 to REF_A at
DUTY_CLAMP1. DUTY_A to DUTY_E has to be in the same order as shown in Figure 7-12.
- DUTY_B configures the duty command for reference
REF_B. There is a step change in reference from REF_A to REF_B at
DUTY_A.
- DUTY_C configures the duty command for reference
REF_C. There is a step change in reference from REF_B to REF_C at
DUTY_B.
- DUTY_D configures the duty command for reference
REF_D. There is a step change in reference from REF_C to REF_D at
DUTY_C.
- DUTY_E configures the duty command for reference
REF_E. There is a step change in reference from REF_D to REF_E at
DUTY_D.
- DUTY_CLAMP2 configures the duty command above
which the reference will be constant at REF_CLAMP2. REF_CLAMP2 configures
this constant reference between DUTY_CLAMP2 and DUTY_OFF2. There is a step
change in reference from REF_E to REF_CLAMP2 at DUTY_E. DUTY_CLAMP2 can be
placed anywhere between DUTY_E and DUTY_OFF2.
- DUTY_OFF2 and DUTY_ON2
configures a hysteresis around reference control input REF_CLAMP2 and
REF_OFF2 as shown in Figure 7-12.
- DUTY_OFF2 configures the duty command above which
the reference will change from REF_CLAMP2 to REF_OFF2.
- DUTY_HYS configures the
hysteresis during every step change at DUTY_CLAMP1, DUTY_A to DUTY_E.