SLVSH86A December 2023 – June 2024 MCT8314Z
PRODUCTION DATA
The current-limit circuit activates if the current flowing through the low-side MOSFETs exceeds the ILIMIT current. Large currents may occur during motor start, high torque events, or stall conditions. The current-limit circuitry utilizes the internal sense FETs on the low-side power FETs of the three phases. Figure 7-22 shows the implementation of current limit circuitry. The ILIM pin sets the ILIMIT by connecting an RLIMIT from ILIM to AGND. Equation 3 calculates the resistor value in Ohms required for a target ILIMIT threshold.
When the current limit activates, the high-side FETs disable until the beginning of the next PWM cycle as shown in Figure 7-23. The low-side FETs can operate in brake mode or coast (high-Z) mode by configuring the ILIM_RECIR bit in the SPI device variant. In the hardware device, the device operates in brake mode when current limiting trips.
Figure 7-23 Cycle-by-Cycle Current-Limit
OperationWhen the current limit activates in synchronous rectification mode, the current recirculates through the low-side FETs while the high-side FETs are disabled as shown in Figure 7-24. When the current limit activates in asynchronous rectification mode, the current recirculates through the body diodes of the low-side FETs while the high-side FETs are disabled as shown in Figure 7-25