SLLSFQ3 January 2023 MCT8329A
PRODUCTION DATA
To prevent sudden changes in the torque applied to the motor which could result in acoustic noise, the MCT8329A device provides the option of limiting the maximum rate at which the duty command input can change in voltage control mode. The closed loop acceleration rate parameter sets the maximum rate at which the duty command (Voltage control reference duty) changes (shown in #SLVSCP26598-2). In the MCT8329A , closed loop acceleration rate is configured through CL_ACC. In closed loop speed and closed loop power control modes, CL_ACC has no impact and the PI loop limit the rate of PWM duty change applied to the motor.