No
action is taken when a CBC_ILIMIT event happens in
this mode.
Note: In CBC_ILIMIT disabled mode and CBC_ILIMIT
report only mode, when the motor is driven at 100%
PWM duty (no switching) and if the current goes
more than the CBC_ILIMIT current threshold, the
gate driver pulls the high side gate driver output
to low momentarily, at the set PWM_FREQ_OUT. To
eliminate such unwanted switching at 100% duty
cycle, the CBC_LIMIT threshold can be set to a
high value more than the expected motor current
during CBC_ILIMIT disabled mode and CBC_ILIMIT
report only mode.