SLLSFQ3 January 2023 MCT8329A
PRODUCTION DATA
The motor is commutated by detecting the zero crossing on the phase which is in Hi-Z state. If the motor is locked, the back-EMF will disappear and MCT8329A will be not able to detect the zero crossing. If MCT8329A is not able to detect zero crossing for LOSS_SYNC_TIMES number of times, LOSS_OF_SYNC event is recognized and action is taken according to the MTR_LCK_MODE. LOSS_OF_SYNC lock can be enabled/disabled by LOSS_OF_SYNC_EN.