SLLSFQ3 January 2023 MCT8329A
PRODUCTION DATA
MCT8329A provides an option of regulating the (input) power instead of motor speed - this input power regulation can be done in two modes, namely, closed loop power control and power limit control. Input power regulation (instead of motor speed) mode is selected by setting CLOSED_LOOP_MODE to 10b. This should be accompanied by setting CONST_POWER_MODE to 01b for closed loop power control or to 10b for power limit control. In either of the power regulation modes, the maximum power that MCT8329A can draw from the DC input supply is set by MAX_POWER - the power reference (POWER_REF in #FIG_UWX_G1B_ZRB).
With REF_PROFILE_CONFIG = 0b, POWER_REF is derived from duty command input (DUTY CMD) from maximum power (configured by MAX_POWER) as shown in #EQUATION-BLOCK_MHJ_1PG_WVB or from the input profiler output (see GUID-E067FB78-4C8A-4ECD-9DB4-6769BF1C2F1D.html. The hysteresis band for the power reference is set by CONST_POWER_LIMIT_HYST. In both the power regulation modes, the minimum power reference is set by MIN_DUTY x MAX_POWER.
In both the power regulation modes, MCT8329A uses the same PI controller parameters as in the speed loop mode. Kp and Ki coefficients are configured through SPD_POWER_KP and SPD_POWER_KI. The PI controller output upper (VMAX) and lower bound (VMIN) saturation limits are configured through SPD_POWER_V_MAX and SPD_POWER_V_MIN respectively. The key difference between closed loop power control and power limit control is in the when the PI controller decides the DUTY OUT (duty cycle of PWM) applied to FETs. In closed loop power control, DUTY OUT is always equal to POWER_PI_OUT from the PI controller output in #FIG_UWX_G1B_ZRB. However, in power limit control, the PI controller decides the DUTY OUT only if POWER_MEAS > POWER_REF + CONST_POWER_LIMIT_HYST. If POWER_MEAS < POWER_REF + CONST_POWER_LIMIT_HYST, the PI controller is not used and DUTY OUT is equal to DUTY CMD. Essentially, in closed loop power control, input power is always actively regulated to POWER_REF whereas, in power limit control, input power is only limited to POWER_REF and not actively regulated to POWER_REF. When output of the power PI loop saturates, the integrator is disabled to prevent integral wind-up.