SBOSA00B December 2019 – August 2020 OPA1637
PRODUCTION DATA
The OPA1637 provides the advantages of a fully differential amplifier (FDA) configuration that offers very low noise and harmonic distortion in a single, low-power amplifier. The FDA is a flexible device, where the main aim is to provide a purely differential output signal centered on a user-configurable, common-mode voltage that is usually matched to the input common-mode voltage required by an analog-to-digital converter (ADC) or class-D amplifier. The circuit used for characterization of the differential-to-differential performance is seen in Figure 7-1.
A similar circuit is used for single-ended to differential measurements, as shown in Figure 7-2.
The FDA requires feedback resistor for both output pins to the input pins. These feedback resistors load the output differentially only if the input common-mode voltage is equal to the output common-mode voltage set by VOCM. When VOCM differs from the input common-mode range, the feedback resistors create single-ended loading. The characterization plots fix the RF (RF1 = RF2) value at 2 kΩ, unless otherwise noted. This value can be adjusted to match the system design parameters with the following considerations in mind: