SBOSAA5C april 2022 – may 2023 OPA2675
PRODUCTION DATA
The first step in a driver design is to compute the peak-to-peak output voltage from the target specifications. This calculation is done using the following equations:
With PL power and VRMS voltage at the load, and RL load impedance, this calculation gives:
With VP peak voltage at the load and the crest factor, CF:
With VLPP: peak-to-peak voltage at the load.
Consolidating Equation 2 through Equation 5 allows the required peak-to-peak voltage at the load function of the crest factor, the load impedance, and the power in the load to be expressed. Thus:
This VLPP is usually computed for a nominal line impedance and can be taken as a fixed design target.
The next step for the driver is to compute the individual amplifier output voltage and currents as a function of VPP on the line and transformer turns ratio. As the turns ratio changes, the minimum allowed supply voltage also changes. The peak current in the amplifier is given by:
With VLPP defined in Equation 6 and RM defined in Equation 8.
The peak current is computed in Figure 8-9 by noting that the total load is 4RM and that the peak current is half of the peak-to-peak calculated using VLPP.
With the required output voltage and current versus turns ratio set, an output stage headroom model allows the required supply voltage versus turns ratio to be developed.
The headroom model (see Figure 8-10) can be described with the following set of equations:
First, as available output voltage for each amplifier:
Or, second, as required single-supply voltage:
The minimum supply voltage for a set of power and load requirements is given by Equation 10, where V1, V2, R1, and R2 are internal to the OPA2675.
Table 8-1 gives V1, V2, R1, and R2 for +12-V operation of the OPA2675.
V1 | R1 | V2 | R2 |
---|---|---|---|
0.9 V | 2 Ω | 0.9 V | 2 Ω |