SBOSAA5C april 2022 – may 2023 OPA2675
PRODUCTION DATA
OPA2675 has four different functional modes set by the A0 and A1 pins. Table 8-2 shows the truth table for the device mode pin configuration and the associated description of each mode.
| A0 | A1 | FUNCTION | DESCRIPTION |
|---|---|---|---|
| 0 | 0 | Full-bias mode (100%) | Both amplifiers are on with the lowest distortion possible |
| 1 | 0 | Mid-bias mode (75%) | Both amplifiers are on with power savings and a reduction in distortion performance |
| 0 | 1 | Low-bias mode (50%) | Both amplifiers are on with enhanced power savings and a reduction of overall performance |
| 1 | 1 | Offline mode | Both amplifiers are off and the output is high impedance |
OPA2675 can be switched between the full-bias and offline mode using just one control bit by tying the A0 and A1 together. If switching between the mid-bias or low-bias modes and the offline mode is required for the application, then either the A0 or A1 pin can be connected to ground and the control pin can be connected to the non-grounded BIAS pin.
The OUT pin of OPA2675 enters high output impedance in offline mode. However, because of the presence of feedback resistor RF (shown in Figure 8-12), the impedance detected by the load going into the OPA2675 is high impedance || RF, making the net impedance as detected from the load equal to RF. The maximum voltage allowed to be incident on the OUT pin and the Inverting Input pin during offline mode is mentioned in the Absolute Maximum Ratings. Figure 8-12 shows the voltage appearing on the Inverting Input pin is a resistor divided value of the voltage on the OUT pin. Make sure that both the absolute maximum limits mentioned for the OUT and Inverting pins are satisfied.