- The thermal pad must be connected
to the most negative supply of the device, V–.
- Prepare the PCB with a top-side
etch pattern, as shown in the attached thermal land pattern mechanical drawing.
Use etch for the leads as well as etch for the thermal land.
- Place the recommended number of
holes (or thermal vias) in the area of the thermal pad, as seen in the attached
thermal land pattern mechanical drawing. These holes are 13 mils (0.013in, or
330.2μm) in diameter. Keep the holes small so that solder wicking through the
holes is not a problem during reflow.
- For optimized performance, place
a small number of the holes under the package and outside the thermal pad area.
These holes provide an additional heat path between the copper land and ground
plane and are 25 mils (0.025in, or 635μm) in diameter. These holes can be larger
because these holes are not in the area to be soldered; therefore, wicking is
not a problem. This configuration is illustrated in the attached thermal land
pattern mechanical drawing.
- Connect all holes, including
those within the thermal pad area and outside the pad area, to the internal
plane that is at the same voltage potential as V–.
- When connecting these holes to
the internal plane, do not use the typical web or spoke via connection
methodology (as Figure 8-16 shows). Web connections have a high thermal resistance connection that is
useful for slowing heat transfer during soldering operations. This configuration
makes the soldering of vias that have plane connections easier. However, in this
application, low thermal resistance is desired for the most efficient heat
transfer. Therefore, connect the holes under the PowerPAD integrated circuit
package to the internal plane with a complete connection around the entire
circumference of the plated through-hole.
- Leave the terminals of the
package and the thermal pad area exposed through the top-side solder mask. Leave
the 13‑mil holes exposed through the thermal pad area. Cover the larger 25‑mil
holes outside the thermal pad area with solder mask.
- Apply solder paste to the exposed
thermal pad area and all of the package terminals.
- With these preparatory steps
completed, the PowerPAD integrated circuit package is simply placed in position
and run through the solder-reflow operation as with any standard surface-mount
component. This processing results in a device that is properly installed.
For detailed information on the
PowerPAD integrated circuit package, including thermal modeling considerations and
repair procedures, see the PowerPAD Thermally Enhanced Package technical
brief, available at www.ti.com.