The following bullets list the
considerations for this design example:
- Input Impedance: The
JFET-input stage of the OPA814 offers gigaohms of input
impedance, and therefore enables the front-end to be terminated with a 1-MΩ
resistor while achieving excellent precision. A 50-Ω resistance can also be
switched in, offering matched termination for high-frequency signals. Thus, the
OPA814 enables the designer to use both 1-MΩ and 50-Ω
termination in the same signal chain.
- Noise: The total noise of
the front-end amplifier is a function of the voltage and current noise of the
OPA814, input termination, and the resistors thermal
noise. However, in 50-Ω mode, the dominant noise source is contributed by the
voltage noise of the OPA814 due to the presence of voltage
noise across the complete bandwidth. Therefore, the total RMS noise of the
front-end amplifier is approximately equal to the voltage noise of the OPA814 over 180 MHz.
The specified input-referred voltage
noise of the OPA814 is 5.3 nV/√Hz; see also Section 6.5. The total integrated RMS noise at the input in a bandwidth of 180 MHz is
given by the following equation:
Equation 2.
The brickwall correction factor of 1.57 is
applied, assuming the bandwidth is limited to 180 MHz with a single-pole RC
filter before digitizing the signal with the ADC. Detailed calculations are
found at TI Precision Labs – Op Amp Noise: Spectral
Density.
-
Optimizing Overshoot: The OPA814 features an internal
slew-boost circuit to deliver fast rise-time in applications that require high
slew rates, such as when configured as a transimpedance amplifier. For
applications where overshoot must be limited, limit the input slew rates by
introducing a series resistance (RS); see also Figure 8-4. Resistor RS forms a low-pass filter with an input capacitance of
approximately 2.5 pF at the noninverting pin of the OPA814,
thus limiting the input slew rate to the amplifier. Figure 8-5 shows how limiting the input slew rate to the amplifier results in good
overshoot performance. Figure 8-6 shows how this configuration achieves a small-signal and large-signal
bandwidth of 180 MHz.