SBAS883A February 2018 – June 2018 OPT3101
PRODUCTION DATA.
Obstacle avoidance for autonomous vehicle navigation is a typical application which can be implemented using this AFE. The system can be optimized to meet the application requirements by optimizing various parameters like illumination current, sub-frame averaging, and auto HDR mode, which are explained in the following sections. Figure 169 shows the interface between the OPT3101 device and an external MCU.