SBOS993A December 2021 – December 2022 OPT4001
PRODUCTION DATA
The OPT4001 device offers several conversion times to select from. Conversion Time is defined as how much time for one measurement to complete and update the results in output register from the time measurement is initiated. Measurement initiation is determined by the mode of operation as specified in Modes of Operation.
CONVERSION_TIME register | Typical Conversion Time |
---|---|
0 | 0.6 ms |
1 | 1 ms |
2 | 1.8 ms |
3 | 3.4 ms |
4 | 6.5 ms |
5 | 12.7 ms |
6 | 25 ms |
7 | 50 ms |
8 | 100 ms |
9 | 200 ms |
10 | 400 ms |
11 | 800 ms |