SLAS763C August 2012 – October 2018 PCM5121 , PCM5122
PRODUCTION DATA.
MSB | LSB | ||||||
1 | 0 | 0 | 1 | 1 | ADR2 | ADR1 | R/ W |
The PCM512x has 7 bits for its own slave address. The first five bits (MSBs) of the slave address are factory preset to 10011 (0x9x). The next two bits of the address byte are the device select bits which can be user-defined by the ADR1 and ADR0 terminals. A maximum of four devices can be connected on the same bus at one time. This gives a range of 0x98, 0x9A, 0x9C and 0x9E. Each PCM512x responds when it receives its own slave address.