SLASE12A July 2014 – October 2014 PCM5242
PRODUCTION DATA.
The PCM5242 is powered through the following pins:
NAME | USAGE / DESCRIPTION |
---|---|
AVDD | Analog Voltage Supply - should be 3.3V. Powers the ADC, PGA, Reference, and Secondary ADC |
DVDD | Digital Voltage Supply - This is used as the I/O voltage control and the input to the onchip LDO. |
CPVDD | Charge Pump Voltage Supply - should be 3.3V |
LDOO | Output from the Onchip LDO. Should be used with a 0.1uF decoupling cap. Can be driven (used as power input) with a 1.8V supply to bypass the onchip LDO for lower power consumption. |
AGND | Analog Ground |
DGND | Digital Ground |
Under certain conditions, the PCM5242 can exhibit some pop on power down. Pops are caused by the device not having enough time to detect power loss and start the muting process.
The PCM5242 has two auto-mute functions to mute the device upon power loss (intentional or unintentional).
XSMT = 0
When the XSMT pin is pulled low, the incoming PCM data is attenuated to 0, closely followed by a hard analog mute. This process takes 150 sample times (ts) + 0.2mS.
Because this mute time is mainly dominated by the sampling frequency, systems sampling at 192kHz will mute much faster than a 48kHz system.
Clock Error Detect
When clock error is detected on the incoming data clock, the PCM5242 switches to an internal oscillator, and continues to the drive the output, while attenuating the data from the last known value. Once this process is complete, the PCM5242 outputs are hard muted to ground.
These auto-muting processes can be manipulated by system designs to mute before power loss in the following ways:
Many systems use a low-noise regulator to provide an AVDD 3.3V supply for the DAC. The XSMT Pin can take advantage of such a feature to measure the pre-regulated output from the system SMPS to mute the output before the entire SMPS discharges. Figure 83 shows how to configure such a system to use the XSMT pin. The XSMT pin can also be used in parallel with a GPIO pin from the system microcontroller/DSP or Power Supply.
The XSMT pin can also be used to monitor a system voltage, such as the 24VDC LCD TV backlight, or 12VDC system supply using a voltage divider created with two resistors. (See Figure 84 )
A timing diagram to show this is shown in Figure 85.
NOTE
The XSMT input pin voltage range is from -0.3V to DVDD + 0.3V.The ratio of external resistors must produce a voltage within this input range. Any increase in power supply (such as power supply positive noise or ripple) can pull the XSMT pin higher than DVDD+0.3V.
For example, if the PCM5242 is monitoring a 12V input, and dividing the voltage by 4, then the voltage at XSMT during ideal power supply conditions is 3V. A voltage spike higher than 14.4V causes a voltage greater than 3.6V (DVDD+0.3) on the XSMT pin, potentially damaging the device.
Providing the divider is set appropriately, any DC voltage can be monitored.
Power-On Reset, DVDD 3.3V Supply
The PCM5242 includes a power-on reset function shown in Figure 86. With VDD > 2.8V, the power-on reset function is enabled. After the initialization period, the PCM5242 is set to its default reset state.
Power-On Reset, DVDD 1.8V Supply
The PCM5242 includes a power-on reset function shown in Figure 87 operating at DVDD=1.8V. With AVDD greater than approximately 2.8V, CPVDD greater than approximately 2.8V, and DVDD greater than approximately 1.5V, the power-on reset function is enabled. After the initialization period, the PCM5242 is set to its default reset state.
The internal digital core of the PCM5242 runs from a 1.8V supply. This can be generated by the internal LDO, or by an external 1.8V supply.
DVDD is used to set the I/O voltage, and to be used as the input to the onchip LDO that creates the 1.8V required by the digital core.
For systems that require 3.3V IO support, but lower power consumption, DVDD should be connected to 3.3V and LDOO can be connected to an external 1.8V source. Doing so will disable the onchip LDO.
When setting IO voltage to be 1.8V, both DVDD and LDOO must be provided with an external 1.8V supply.
The PCM5242 offers two power-save modes; standby and power-down.
When a clock error (SCK, BCK, and LRCK) or clock halt is detected, the PCM5242 automatically enters standby mode. The DAC and line driver are also powered down. The device can also be placed in standby mode via software command.
When BCK and LRCK remain at a low level for more than 1 second, the PCM5242 automatically enters power-down mode. Power-down mode disables the negative charge pump and bias/reference circuit, in addition to those disabled in standby mode. The device can also be placed in power-down mode via software command.
The detection time of BCK and LRCK halt can be controlled by Page 0, Register 44, D(2:0).
When expected Audio clocks (SCK, BCK, LRCK) are applied to the PCM5242, the device starts its powerup sequence automatically. The detection time for BCK and LRCK halt is programmable.
Register | Description |
---|---|
Page 0, Register 2, D(4) | Software standby mode command |
Page 0, Register 2, D(0) | Software power-down command |
Page 0, Register 2, D(4) and D(0) | Software power-up sequence command (required after software standby or power-down) |
Page 0, Register 44, D(2:0) | Detection time of BCK and LRCK halt |