SBAS495D June 2010 – August 2021 PCM9211
PRODUCTION DATA
MSB | LSB | ||||||
1 | 0 | 0 | 0 | 0 | ADR1 | ADR0 | R/ W |
The PCM9211 has seven bits for its own slave address. The first five bits (MSB) of the slave address are factory-preset to '10000'. The next two bits of the address byte are selectable bits that can be set by MDO/ADR0 and MS/ADR1. A maximum of four PCM9211s can be connected on the same bus at one time. Each PCM9211 responds when it receives its own slave address.