SLASEJ4C April 2017 – February 2023 PGA460
PRODUCTION DATA
The rectifier, peak extractor, and low-pass filter DSP blocks demodulate the echo signal while outputting a base-band representation to be compared against the programmed thresholds. These blocks are defined as:
On power up the PGA460 device calculates the values of the filter coefficients and places them in the LPF_A2_xSB and LPF_B1_xSB registers, respectively. The user can overwrite the values in these registers and reconfigure the filter. In this case, the PGA460 device does not take any action. However, if the LPF_CO bit is changed, the coefficient calculation sequence must be rerun and the device repopulates these registers.