SLOS412E April 2003 – November 2024 RC4580
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The common-mode rejection ratio (CMRR) of an amplifier is a measure of how well the device rejects unwanted input signals common to both input leads. The CMRR is found by taking the ratio of the change in input offset voltage to the change in the input voltage, then converting to decibels. Ideally the CMRR is infinite, but in practice, amplifiers are designed to have the CMRR as high as possible. The CMRR of the RC4580 device is 110dB.