SBOSA80 December 2021 REF20-Q1
PRODUCTION DATA
The voltage reference for this application must have the following features:
For this design, the REF2030-Q1 is used. The REF20xx-Q1 topology is as shown in the Section 9.2 section.
The REF2030-Q1 is an excellent choice for this
application because of its dual output. The
temperature drift of
8 ppm/°C and initial accuracy of 0.05% make the
errors resulting from the voltage reference
minimal in this application. In addition, there is
minimal mismatch between the two outputs and both
outputs track very well across temperature, as
shown in Figure 10-4 and Figure 10-5.